{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What causes an SLF3 fault on an ATV600 or ATV900 series drive?

Issue:
What causes an SLF3 fault on an ATV600 or ATV900 series drive?

Product Line:
ATV600 / ATV900 / Altivar

Environment:
Altivar Machine

Cause:
Hardware profile change after programming.

Resolution:
SLF3 occurs when the drive has programming entered to support controlling the drive via the keypad, and the keypad has been removed.  This fault indicates that there is programming in the drive to support hardware (the keypad) that the drive can not see connected.
To correct this, either change the programming of the drive so that is it not using the keypad to control the drive, or make sure the keypad remains connected to the drive any time the drive has power.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: