{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV320 Drives RJ45 connector pinout for CANopen option card VW3A3608.
Issue:
ATV320 CANopen pinouts for the RJ45 connector.

Product Line:
ATV320 with option card VW3A3608

Environment:
All

Cause:
RJ45 connector pinout on option card VW3A3608.

Resolution:

Pin Layout
Pin 1 = CAN_H
Pin 2 = CAN_L
Pin 3 = CAN_GND

See the attached documents for more programming and CANopen information. Page 31 of NVE41309 12/2017
https://www.se.com/us/en/download/document/NVE41309/

Schneider Electric Saudi Arabia