{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

TeSys T LTMR..EBD doesn't respond to network commands

Issue:
Tesys T does not respond to command via Ethernet. IP address can be pinged, registers can be read, and Tesys is configured for network control but will not respond to network commands.

Product Line:
LTMR Tesys T motor controllers.

Environment:
Products sold in the US

Cause:
Tesys was in configuration mode, not run mode.

Resolution:
The Tesys will not run in configuration mode. In run mode you only have command menu under the device tab in the latest DTM Library. Ensure you have the latest DTM Library Installed. This will allow you to place Tesys in Run mode and verify proper operation.

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range:
Category: