{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Looking for handle kit for B frame Powerpact breaker for through-the-door breaker operation?

Issue:

Throug the door handle kit for B Frame powerpact breaker.

Product Line:
PowerPact B breakers

Environment:
PowerPact B-Frame Moulded Case Circuit Breakers

Cause:
It is often necessary  operate breakers from outside of the enclosure they are installed in when they are not used in a Schneider panelboard

Resolution:

You can use the following;

LV426932 or LV426933

Schneider Electric Saudi Arabia

Explore more
Range:
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: