{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to solve the "The protocol Modbus installed for Vijeo-Designer Lite is too old" error in Vijeo-Designer Lite version 1.3
Issue:
When opening a project in Vijeo-Designer Lite version 1.3, the error "The protocol Modbus installed for Vijeo-Designer Lite is too old" comes up and the project does not open.

Product Line:
HMI, Magelis

Environment:
Vijeo-Designer Lite version 1.3

Resolution:
To solve this error it is required to install the Service Pack 1 available for Vijeo-Designer Lite version 1.3. You can use this link to get it:
https://www.se.com/ww/en/download/document/Vijeo+Designer+Lite+V1.3+SP1/

Schneider Electric Saudi Arabia