{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to read data from MX EcoDrive frequency converter over Modbus RTU?

Article available in these languages: Czech

MX drives are totally different than Altivar drives. See modbus manual for MX eco drives in the attachment. Page 6 shows all important information and page 16 example with function code 17. If you want only to read parameters from MX eco, (not sending commands), then use function code 3 - read holding registers

The modus request will look: (each byte separated by "-")
Slave address - 16#03 - 16#00 - 16#FA - 16#00 - 16#02 - CRCLow - CRCHi

16#00FA is the address of the status word ZTW and 16#0002 means that 2 words will be read:
ZTW (status word) from address 16#00FA
Fact (actual frequency) from address 16#00FB

If you need to read more data, use another request.
Full request and response with function code 3 shown on page 32

Schneider Electric Saudi Arabia

Attachment(s)
8_P01_034_EN_00-00b.pdf [1.55 MB]