Search FAQs
Can the real time clock information (date and time) be set over a communication network in the Altivar Process Drives?
Issue:
Setting up real time clock information (date and time) over a communication network in the Altivar Process Drives.
Product Line:
Altivar Process
ATV630, ATV650, ATV660, ATV680
ATV930, ATV950, ATV960, ATV980
ATV630, ATV650, ATV660, ATV680
ATV930, ATV950, ATV960, ATV980
Environment:
Any serial communication protocol
Cause:
Internal memory address for date and time are not included in the publically available documents.
Resolution:
The Date and Time in the Altivar Process drives can be entered via the HMI keypad in Menu 8 [My Preferences] under the Date/Time Settings submenu.
They can also be read or modified over many of the serial communication protocols available.
They can also be read or modified over many of the serial communication protocols available.
Name | Type | Address | Binary representation | |||
hour | minute | |||||
DAY | UINT | 7391 | binary: | xxxx.xxxx. | xxxx.xxxx | |
year | month | day | ||||
TIME | UINT | 7392 | binary: | xxxx.xxx | x.xxx | x.xxxx |
Released for:Schneider Electric Saudi Arabia
Explore more
Category:
Range:
Explore more
Category:
Range: