Search FAQs
Can NetShelter horizontal cable managers be mounted back-to-back?
Issue:
A customer is asking if the horizontal cable managers can be mounted back-to-back.
Product Line:
NetShelter Horizontal Cable Managers
Environment:
AR8600A, AR8602A, AR8603A, AR8605, AR8606, AR8612
Cause:
In some installations it may be advantageous to mount the horizontal cable managers on both sides of the mounting rail.
Resolution:
Yes, the horizontal cable managers can be mounted back-to-back. Please see the installation sheet: http://www.apc.com/salestools/BFER-8KYNMU/BFER-8KYNMU_R2_EN.pdf
A customer is asking if the horizontal cable managers can be mounted back-to-back.
Product Line:
NetShelter Horizontal Cable Managers
Environment:
AR8600A, AR8602A, AR8603A, AR8605, AR8606, AR8612
Cause:
In some installations it may be advantageous to mount the horizontal cable managers on both sides of the mounting rail.
Resolution:
Yes, the horizontal cable managers can be mounted back-to-back. Please see the installation sheet: http://www.apc.com/salestools/BFER-8KYNMU/BFER-8KYNMU_R2_EN.pdf
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: