Issue:
Maximum power consumption rating of the 24V supply for ATV630 drive.
Product Line:
Altivar 630
Environment:
All
Cause:
Power consumption
Resolution:
- +24 Vdc
- Tolerance: minimum 20.4 Vdc, maximum 27 Vdc
- Current: maximum 200 mA for both 24 Vdc terminals
- Terminal protected against overload and short-circuit
- In Sink Ext position, this supply is powered by external PLC supply
+24 Vdc
Tolerance: minimum 20.4 Vdc, maximum 27 Vdc
Current: maximum 200 mA for both 24 Vdc terminals
Terminal protected against overload and short-circuit
In Sink Ext position, this supply is powered by external PLC supply
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Saudi Arabia