{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the Hot Fixes for Unity Pro v10.0 to configure the PRM with M580?

Issue
This resolution clarifies the minimum hot fixes to be installed in Unity Pro v10.0 that guarantee a correct value of the variables from the PRM.

Product Line
EcoStruxure Control Expert, M580, PRM (TCSEGPA23F14F)

Environment
Unity Pro v10.0, BMEP581020 v2.50, PRM

Resolution
The PROFIBUS Remote Master (PRM) is a Profibus gateway that can also be used with M580 and the variables of the slaves are populated by a Device Derived Data Type. So, you need to install the hot fixes below to have a right order of bytes on Device DDT variables of the module and also when you connect the PRM to the BMENOC0301/0311/0321, modify the subnet mask or gateway address in the DHCP server:

Schneider Electric Saudi Arabia