{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why MCL or CID file is hidden or gray in Px4x relay's setting file & please share the reason?
Our latest version Px4x relays that will support both edition 1 and 2.
The selection will be done via the front panel of the relay under system, you can choose either edition 1 or 2.

If they choose edition 1 then only mcl file is available.
If you have chosen edition 2, the relay supplied with The relay both edition 1 and 2.

When reay connected to the Easergy Studio, the option cid or mcl is available as per the selection in the relay during ordering

Hence you may see the MCL or CID file Hidden or showing gray color during communication with Easergy studio

Schneider Electric Saudi Arabia