Search FAQs
Is there an EM4900 driver for PME 8.0 and 8.1?
Issue
Unable to find an EM4900 driver for PME 8.0 and 8.1.
Product Line
Power Monitoring Expert 8.0
Power Monitoring Expert 8.1
Environment
Power Monitoring Expert
Cause
The EM4900 driver on PME 8.0 and PME 8.1 no longer exist.
Resolution
Upgrade to PME 8.2 that has the EM4900 driver available and uses the same licenses as PME 8.0 and 8.1.
To download the EM4900 driver for PME 8.2, click on this link
https://schneider-electric.app.box.com/s/h56qxurz6wj65wmi80pd3bky62hlv942
For links to the installation files to Upgrade to PME 8.2, please refer to FA312664.
Note: The EM4900 driver is native to all versions of PME after PME 8.2.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: