Issue:
CAD drawings request for the Process Drive HMI (keypad), part# VW3A1111
Product Line:
VW3A1111
Environment:
All
Cause:
Need CAD drawings
Resolution:
Please redirect yourself to the following link:
https://www.se.com/us/en/product/VW3A1111/graphic-display-terminal---240-x-160-pixels---ip65/
You will be able to download the CAD file there.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for:Schneider Electric Saudi Arabia