Search FAQs
On an ATV320, how is the fault history accessed?
Issue:
Access of fault history on the ATV320.
Product Line:
Altivar 320
Environment:
All
Cause:
Need to view fault history
Resolution:
The fault history is not available from the integral keypad/display. It is only accessible through a connected graphic keypad or through SoMove software.
Using the VW3A1101 or VW3A1111 graphic keypad, under the Drive Menu, select MONITORING, then DIAGNOSTICS, then FAULT HISTORY. The last 8 faults are listed with most recent at top. Select the fault to access status info at time of fault.
Using SoMove, select the Errors detection tab. In the left side panel, the History is listed Error n-1 (most recent) through Error n-8. Select a fault for details.
Troubleshooting help is offered in the program manual Diagnostics and Troubleshooting section.
The Programming manual can be accessed here:
https://www.se.com/ww/en/download/document/NVE41295/
Access of fault history on the ATV320.
Product Line:
Altivar 320
Environment:
All
Cause:
Need to view fault history
Resolution:
The fault history is not available from the integral keypad/display. It is only accessible through a connected graphic keypad or through SoMove software.
Using the VW3A1101 or VW3A1111 graphic keypad, under the Drive Menu, select MONITORING, then DIAGNOSTICS, then FAULT HISTORY. The last 8 faults are listed with most recent at top. Select the fault to access status info at time of fault.
Using SoMove, select the Errors detection tab. In the left side panel, the History is listed Error n-1 (most recent) through Error n-8. Select a fault for details.
Troubleshooting help is offered in the program manual Diagnostics and Troubleshooting section.
The Programming manual can be accessed here:
https://www.se.com/ww/en/download/document/NVE41295/
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: