Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which SoMachine / EcoStruxure Machine Expert PLCs use the PLC Usb Driver?

Article available in these languages: Japanese

Issue
Which SoMachine / EcoStruxure Machine Expert PLCs use the PLC Usb Driver?

Product Line
SoMachine v2, v3, up to v4.3
EcoStruxure Machine Expert

Environment
Windows Driver for USB cable connection to Modicon PLC from SoMachine

Resolution
The PLC USB Driver Suite is only used by the following SoMachine controllers (M258, LMC058, and ATV-IMC).
For EcoStruxure Machine Expert, the Modicon M262 PLCs also use the PLC Usb Driver.

When connected to those controllers via USB, they will appear up under "Modems" under the device manager and establish a 90.0.0.1 connection in the PLC-USB driver.

M258, LMC058, ATV-IMC, M262 PLCs use the PLC USB driver and shows under Modems in the Device Manager
Windows Device Manager Modems category

Schneider Driver Management Properties

As for other PLCs:
The M238, M241 and M251 require the installation of a component called "GatewayOptionalDrivers" which contains the USB driver files needed for these PLCs
This is installed by SoMachine Configuration Manager in a Default installation of the software.
In EcoStruxure Machine Expert, the GatewayOptionalDrivers component is also installed as part of a default installation from the "Schneider Electric Software Installer" Tool.

M238, M241 and M251 families do not use the PLC USB driver and only shows under LibUsb-Win32 in the Windows Device Manager:
Windows Device Manager - LibUsb-Win32 category

Schneider Electric Saudi Arabia

Attachment(s)
M258_ATVIMC_LMC058_DeviceManagerModem.jpg [105.81 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.