{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV630 - freewheel stop functionality.
Issue:
Customer has a ATV630 and is controlling through Ethernet. It is setup in hand to run with the logic inputs. They want to be able to stop the drive while in Coms with a logic input. They do not want to use the STOA and/or STOB, because they do not want to have to power cycle the drive. He was wondering if he could assign a digital input to nst , and stop the drive, even while running totally ( start/stop and speed control) through Communications?

Product Line:
ATV630 drives

Environment:
Ethernet IP

Cause:
n/a

Resolution:
According to Engineering, to stop the drive with Comms, with a log input:
Use 3-wire control (TCC=3-wire control).
DI1 must be ON to run the drive, when you open it, you stop the drive (-->NST).

Schneider Electric Saudi Arabia