{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is specfic amount of time that the ATV212 is capable of maintaining running in the event of a momentary power loss?
Issue:
Does the ATV212 have a power loss ride through?

Product line:
ATV212, Altivar 212

Environment:
all

Cause:
Specifications shows the drive can maintain run during a power loss or dip.

Resolution:
The drive can maintain a run in the event of a power loss or dip however too many factors determine for how long of a period this can maintain.  Some of the factors affecting the time are:
Efficiency of each motor pole
The inertia of the load
The size of the drive

The only way to confirm an exact amount of time is to conduct a test on the specific drive and motor installation.

Schneider Electric Saudi Arabia