Search FAQs
What does class S1 and S2 mean for a HV circuit breaker ?
IEC 62271‐100 defines two separate class according to the type of the system.
circuit-breaker class S1
circuit-breaker intended to be used in a cable system
circuit-breaker class S2
circuit-breaker used in a line-system
The type tests and the specifications are different if the circuit breaker is defined S1 or S2 class.
Our HV circuit breakers (LF,SF, Evolis, Easypact EXE) are S1 class
circuit-breaker class S1
circuit-breaker intended to be used in a cable system
circuit-breaker class S2
circuit-breaker used in a line-system
The type tests and the specifications are different if the circuit breaker is defined S1 or S2 class.
Our HV circuit breakers (LF,SF, Evolis, Easypact EXE) are S1 class
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: