Search FAQs
What is the maximum size of the CoreDB in Easergy T300? What is the maximum number of variables that the T300 can handle?
- HU250 module includes 1GBit SDRAM memory and each SC150 has 4Mo.
- The limit of the T300 system comes from the capacity to connect devices (24 SC150 max) upon which the communication could get saturated.
- However, there are no specific limits concerning the number of variables.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: