Issue:
Customer wants to add a second blue pilot light to the ERMS function on output #3.
Product Line:
Circuit Breakers
Environment:
Breaker digital systems IO module
Resolution:
Although the O3 contact may be wired to the ERMS Selector Switch which is illuminated, An additional pilot light may be wired in parallel.
The output contacts are not self powered.
The output contacts can have parallel loads as long as you don't exceed the amperage and voltage rating of the output contact (bistable relay).
The rated load is 5A at 250Vac.
Max Switching Voltage 380 Vac, 125 Vdc
Max Switching Current 5 Amps
Maximum cable length 10 meters (33 feet)
Please see attached document for complete listed ratings.
Customer wants to add a second blue pilot light to the ERMS function on output #3.
Product Line:
Circuit Breakers
Environment:
Breaker digital systems IO module
Resolution:
Although the O3 contact may be wired to the ERMS Selector Switch which is illuminated, An additional pilot light may be wired in parallel.
The output contacts are not self powered.
The output contacts can have parallel loads as long as you don't exceed the amperage and voltage rating of the output contact (bistable relay).
The rated load is 5A at 250Vac.
Max Switching Voltage 380 Vac, 125 Vdc
Max Switching Current 5 Amps
Maximum cable length 10 meters (33 feet)
Please see attached document for complete listed ratings.
Released for:Schneider Electric Saudi Arabia