Search FAQs
Can the AR8395 busbar install into a NetShelter SV? The busbar installs at three points, but the cabinet only has two accessory mounting brackets.
Issue:
The AR8395 busbar has three installation points.
Product Line:
NetShelter SV, AR8395
Environment:
All models, all serial numbers.
Cause:
NetShelter SV cabinets ship with two accessory mounting brackets.
Resolution:
The AR8395 busbar is compatible with NetShelter SV cabinets, but it does require an extra accessory bracket (AR824002).
See attached file.
The AR8395 busbar has three installation points.
Product Line:
NetShelter SV, AR8395
Environment:
All models, all serial numbers.
Cause:
NetShelter SV cabinets ship with two accessory mounting brackets.
Resolution:
The AR8395 busbar is compatible with NetShelter SV cabinets, but it does require an extra accessory bracket (AR824002).
See attached file.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: