Search FAQs
Video : How can I configure a Profibus STB island and save the GSD file?
Issue
GSD file contains the description of Profibus DP and you can generate one by Advantys for STBNDP2212
Product Line
Advantys STB, TCSEGPA23F14F (PRM), EcoStruxure Control Expert (formerly known as Unity Pro)
Environment
TCSEGPA23F14F, Unity Pro v13.0, STBNDP2212., Advantys v11
Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. This video will show you how to configure a STBNDP2212 with 3 CanOpen slaves and save the GSD file to be imported by Profibus Master.
GSD file contains the description of Profibus DP and you can generate one by Advantys for STBNDP2212
Product Line
Advantys STB, TCSEGPA23F14F (PRM), EcoStruxure Control Expert (formerly known as Unity Pro)
Environment
TCSEGPA23F14F, Unity Pro v13.0, STBNDP2212., Advantys v11
Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. This video will show you how to configure a STBNDP2212 with 3 CanOpen slaves and save the GSD file to be imported by Profibus Master.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: