Issue:
Need to confirm that the Altivar Process drive is recognizing the digital inputs.
Product line:
ATV600, ATV900, Altivar Process
Environment:
n/a
Cause:
Troubleshooting drive
Resolution:
Push the Home button to get to the Main Menu.
From the Main Menu, navigate to Display -> I/O Map -> Digital Input Map.
It will now display the status of the STOA, STOB and Digital Inputs 1 thru 8. The contact is closed if the Input shows High (or up). The contact is open if the input shows Low (or down).
Note: From this menu, highlight and enter each input to check which functions are assigned to it.
Need to confirm that the Altivar Process drive is recognizing the digital inputs.
Product line:
ATV600, ATV900, Altivar Process
Environment:
n/a
Cause:
Troubleshooting drive
Resolution:
Push the Home button to get to the Main Menu.
From the Main Menu, navigate to Display -> I/O Map -> Digital Input Map.
It will now display the status of the STOA, STOB and Digital Inputs 1 thru 8. The contact is closed if the Input shows High (or up). The contact is open if the input shows Low (or down).
Note: From this menu, highlight and enter each input to check which functions are assigned to it.
Released for:Schneider Electric Saudi Arabia