{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What happens when the optional installed EPO is triggered on the single phase Symmetra?
Product Line
Symmetra LX
Symmetra RM
Symmetra Power Array

Resolution
When the EPO on the single phase Symmetras is triggered it will cause the System Enable switch (on/off switch) to physically move to the "off" position. Regardless of what state the UPS is in (On battery, On line, In Bypass) the Symmetra will immediately be powered off entirely. This includes all load attached.

Schneider Electric Saudi Arabia