Search FAQs
Can we adjust the overload relay while the motor is running?
Issue:
Customer wants to adjust the LR9F overload while the motor is running.
Product line:
LRD, LR9, LR9F, 9065 solid state, SSOLR
Environment:
All solid state or overloads with adjustable dials.
Resolution:
It is recommended to stop the motor and then adjust the overload settings.
Customer wants to adjust the LR9F overload while the motor is running.
Product line:
LRD, LR9, LR9F, 9065 solid state, SSOLR
Environment:
All solid state or overloads with adjustable dials.
Resolution:
It is recommended to stop the motor and then adjust the overload settings.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: