{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to check the Micrologic type E 's battery status?

1. Micrologic is not connected to the auxiliary 24V DC power supply: by pressing the test/reset button the red LEDs should light up if the battery is charged, but not the display. In this situation it is shown that the battery is still charged by lighting up the Ir, Isd, Ig, Ap LEDs.

2. Micrologic is connected to the auxiliary 24V DC power supply and the display is switched on: In this case, the status of the battery is shown on the display in percentage (100%, 80%, 60%, 40%, 20% or 0%).

Schneider Electric Saudi Arabia