Issue:
When you first connect the battery there is a delay before the unit can start on battery with no utility power present.
Product Line:
Smart-UPS
Environment:
SMTL750RM2UC, SMTL1000RM2UC, SMTL1500RM3UC - All Serial Numbers
Cause:
If the UPS is not connected to AC Power, then there will be up to a 1 minute delay between the initial connection of the battery and the UPS being ready to start.
Resolution:
Wait 1 minute before pressing the ON key, or connect the UPS to AC power to eliminate the delay.
Released for:Schneider Electric Saudi Arabia