PM5340 meter restarts when trying to configure Modbus, Ethernet or BACnet through the meter HMI.
This is known issue and it is fixed in the firmware V2.1.37.
Use DLF3000 tool to upgrade the firmware and Default IP address of the meter is 85.16 as the first two values of the IP address, then convert the last two hexadecimal values of the MAC address to decimal and use this as the last two values of the IP address.
Ex: MAC address =00:80:67:82:B8:C8
Default IP =85.16.184.200
Refer the KB article FA236782 for DLF3000 upgrade procedure
This is known issue and it is fixed in the firmware V2.1.37.
Use DLF3000 tool to upgrade the firmware and Default IP address of the meter is 85.16 as the first two values of the IP address, then convert the last two hexadecimal values of the MAC address to decimal and use this as the last two values of the IP address.
Ex: MAC address =00:80:67:82:B8:C8
Default IP =85.16.184.200
Refer the KB article FA236782 for DLF3000 upgrade procedure
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.