{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can I save and send a recipe automatically in EcoStruxure Operator Terminal Expert (formerly known as Vijeo XD V3.0)?
Issue:
Looking for a way to save and send a recipe automatically

Product Line:
HMISTO705, HMISTO715, HMIST735, EcoStruxure Operator Terminal Expert

Resolution:
The HMISTO705, HMISTO715 and HMISTO735 does not have the ability to retain internal variable on a power cycle.

As a workaround it is possible to mimic this behavior using a recipe. In the script seen below, when the Runtime Starts, a recipe is loaded and the same recipe is saved every 15 seconds.

Schneider Electric Saudi Arabia