Search FAQs
Data Center Expert | What types of Administrative system level alerts are sent?
Issue:
Administrative alerts in Data Center Expert
Product Line:
EcoStruxure IT Data Center Expert
StruxureWare Data Center Expert
Environment:
EcoStruxure IT Data Center Expert (DCE)
StruxureWare Data Center Expert (DCE)
Cause:
Administrative alerts are pre-defined in DCE. These alerts will be sent when an event below occurs and email is configured with a local or LADP/AD user account.
Resolution:
Here is a list of all the possible system level notifications a user could receive from DCE:
Please note that to be notified for any of these alerts, the user / administrative account must have an e-mail associated with their login either in DCE or, if DCE is configured to use them, in an associated Active Directory / LDAP account.
Administrative alerts in Data Center Expert
Product Line:
EcoStruxure IT Data Center Expert
StruxureWare Data Center Expert
Environment:
EcoStruxure IT Data Center Expert (DCE)
StruxureWare Data Center Expert (DCE)
Cause:
Administrative alerts are pre-defined in DCE. These alerts will be sent when an event below occurs and email is configured with a local or LADP/AD user account.
Resolution:
Here is a list of all the possible system level notifications a user could receive from DCE:
Please note that to be notified for any of these alerts, the user / administrative account must have an e-mail associated with their login either in DCE or, if DCE is configured to use them, in an associated Active Directory / LDAP account.
System Alert | Alert Description |
Cancelled Backup | If a backup is in progress and someone cancels it through DCE User Interface. |
Critical Communications Error | If a NetBotz 300-500 series appliance drops offline (does not apply to SNMP). |
Drive Issues (Enterprise server only) | - If one of the hard drives in the RAID is bad or rebuilding (the state it will be in after you insert a replacement drive). |
Email Tests | The test email sent when setting your SMTP (email server) settings. |
Failed Backup | If a backup starts successfully, but is unable to complete (runs out of disk size, share drops offline, etc...) |
Failed Schedule Export | Same as "Failed Backup" but for scheduled exports |
Purging | When the disk is being purged because the usage has reached the limit set in the user interface |
Reboot | When the server is rebooted. |
Storage Repository Offline | When DCE uses an external storage repository and it drops offline. |
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: