How to acknowledge alarms so the front panel LED will stop blinking on a CM4000?
Product Line
CM4000
Environment
Front Display
Cause
Each alarm also has a priority level. Use the priorities to distinguish between events that require immediate action and those that do not require action.
Medium priority—if a medium priority alarm occurs, the LED flashes and a message displays only while the alarm is active. Once the alarm becomes inactive, the LED stops flashing.
Low priority—if a low priority alarm occurs, the LED on the display flashes only while the alarm is active. No alarm message is displayed.
No priority—if an alarm is setup with no priority, no visible representation will appear on the display. Alarms with no priority are not entered in the Alarm Log. See Logging for alarm logging information. [Page 85]
Resolution
The LED will flash while the alarm is active. Once the alarm has been cleared, then the LED will cease flashing.
Only high priority alarms need to be acknowledged. If this alarm is a nuisance it can alternatively be set to no priority.
To acknowledge high priority alarms from the front display:
2. --> View Alarms
3. --> Active Alarms List
If there is an active, unacknowledged high priority alarm, the CM4000 will ask you to acknowledge the alarm. Otherwise, the LED will flash for all active alarms with a priority.
To set alarm priority from the front display:
2. --> Setup
3. Enter Password ****
5. Arrow down to --> Alarm
6. --> Edit Parameters
7. --> Disturbance
8. Arrow down to edit Priority
Released for: Schneider Electric Saudi Arabia


Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.