Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What can cause an ASF or angle error on the ATV630 and ATV930 Process drives?
Issue:
Posible cause for an ASF or angle error on the ATV630/930 drives.

Product Line:
ATV630 and ATV930 Process drives

Environment:
All 

Cause:
For synchronous motors , the wrong speed loop setting when the reference goes to zero.

Resolution:
Verify the speed loop parameters
Verify the motor phases and the maximum current allowed by the drive. 

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: