{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause an CFI3 or Pre-setting transfer error on the ATV630 and ATV930 Process Drives?

Article available in these languages: Spanish

Issue:
CFI3 or Pre-setting transfer error causes on the ATV630 and ATV930 Process Drives.

Product Line:
ATV630 and ATV930 Process Drives

Environment:
All

Cause:
• The configuration transfer to the drive was not successful or interrupted.
• The stored pre-set was loaded from an different firmware (MCP/MCE), with additional, less parameters.

Resolution:
Principle
The pre-setting transfer error occurs if a pre-set file could not be loaded to the device, or the configuration is not compatible.
Probable cause
• The configuration transfer to the drive was not successful or interrupted.
• The stored pre-set was loaded from an different firmware (MCP/MCE), with additional or less parameters.

Remedy
• Load a compatible configuration.
• Check the pre set file
• Use SoMove to transfer pre-set to the device
• perform a factory setting

Schneider Electric Saudi Arabia

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: