{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PM5560 changes the IP address to Default IP (85.16.xx.xx)

Article available in these languages: Spanish

Issue
PM5560 changes the IP address to Default IP (85.16.xx.xx)

Product Line
PM5560
PM5563
PM5561


Environment
Ethernet Communication

Resolution
PM5560 meter is designed in a way that if the meter detects IP conflict or (duplicate IP detection) then the device will automatically fall back to default IP address.

Default IP address is use 85.16 as the first two values of the IP address, then convert the last two hexadecimal values of the MAC address to decimal and use this as the last two values of the IP address
Example: MAC address = 00:80:67:82:B8:C8
Default IP address = 85.16.184.200

You can observe this behavior in the meter HMI and system log.

Log in to meter using FTP - Navigate the FW folder and check the system log for the below events :
20 07/11/2016 20:20:39.499: fdr: duplicated IP configured, fall back to default IP

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: