{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is a SCF3 fault on a ATV320 drive?

Article available in these languages: Spanish, Turkish

Issue:
ATV320 drive showing an SCF3 fault

Product Line:
ATV320

Environment:
SCF3

Cause:
n/a

Resolution:
This is a ground Short Circuit fault.
Recheck all the motor parameters. Check all the cables connecting the drive to the motor, and the motor insulation. Reduce the switching frequency. Check the adjustment of speed loop and/or brake, if applicable. Increase the Time to Restart ( ttr parameter in Set menu) - if there is a brake?  Disconnect the motor leads and then turn off the OPL and try to run the drive open circuit and see if it still faults.  If it does, the drive appears to be inoperative

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: