Issue:
Could not find the replacement fan for the Altistart 22
Product Line:
Altistart 22
Environment:
All models and serial numbers
Cause:
Replacement cooling fan.
Resolution:
Smaller ATS22 units do not have a fan built-in, but can have an external fan accessory.
For larger ATS22 units, there is a built-in fan, but these are not available in the US.
Could not find the replacement fan for the Altistart 22
Product Line:
Altistart 22
Environment:
All models and serial numbers
Cause:
Replacement cooling fan.
Resolution:
Smaller ATS22 units do not have a fan built-in, but can have an external fan accessory.
Control supply voltage | Part Numbers | Optional Fan |
220VAC | ATS22D17Q…D47Q | VW3G22400 |
ATS22D17S6…D47S6 | ||
ATS22D62Q…D88Q | VW3G22401 | |
ATS22D62S6…D88S6 | ||
ATS22C11Q…C17Q | VW3G22402 | |
ATS22C11S6…C17S6 | ||
110VAC | ATS22D17S6U…D47S6U | VW3G22U400 |
ATS22D62S6U…D88S6U | VW3G22U401 | |
ATS22C11S6U…C17S6U | VW3G22U402 |
For larger ATS22 units, there is a built-in fan, but these are not available in the US.
Control supply voltage | Part Numbers | Built-in Fan |
220VAC | ATS22C21Q...C41Q | VZ3V22D1220V |
ATS22C21S6..C41S6 | ||
ATS22C48Q…C59Q | VZ3V22E1220V | |
ATS22C48S6…C59S6 | ||
110VAC | ATS22C21S6U...C41S6U | VZ3V22D1110V |
ATS22C48S6U...C59S6U | VZ3V22E1110V |
Released for:Schneider Electric Saudi Arabia