{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the IO module be used for ground fault alarm?
Issue:
Can the IO module be used for ground fault alarm with Masterpact and Powerpact breakers?

Product Line:
Circuit Breakers

Environment:
Powerpact P and R, Masterpact NT and NW.  With P and H trip units.

Resolution:
Yes. EcoStruxure Power Commission software version 2.12 released March 29, 2019  has GF alarm functionality through FW update to the IO module. EcoStruxure Power Commission software prior to version 2.12 does not have GF alarm functionality.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: