Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What is the U-height of the upper and lower ducts on AR7715?
Issue:
Customers want to know overall height of the AR7715, plus the equipment they're installing into it. 

Product Line:
AR7715

Environment:
All versions and serial ranges.

Cause: 
A customer needs to determine how much U-space the side airflow duct kit uses, so they know how much available space that leaves in the caibnet. 

Resolution:

The ducts of the AR7715 take 2U each, for a total of 4U. Adding 4U to the height of the switch installed inside the AR7715 gives the total U-height. 

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: