{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Transferring a Unity application through a VPN could fail.
Issue
Transferring a Unity application through a corporate VPN could fail.

Product Line
Unity

Environment
Windows 10


Resolution
Attempts to transfer a Unity application (download or upload) from an M580 PLC using the Ethernet port on either the CPU,
BMXNOx0xxx Ethernet module (i.e., BMXNOR0200, etc.) or BMENOx0xxx Ethernet module (i.e., BMENOC0402, etc.) that
is connected to Unity through both a corporate network and VPN, could fail. This can happen if a large lag time occurs in the
TCP/IP connection while Unity is waiting for a response from the PLC during the transfer process.

The issue can be resolved by running the appropriate attached registry edit batch file.
This will disable the optimization for the transfer process between Unity and the PLC.  As a result, the time to complete the transfer
process could be longer.


Schneider Electric Saudi Arabia

Attachment(s)
Unity fix for VPN Upload_Dowload Failure.7z [400 Bytes]