{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to program an ATV212 for use in an S-Flex?

Article available in these languages: Spanish

Issue:
Program an ATV212 for use in an S-Flex.

Product Line:
ATV212 S-Flex

Environment:
All

Cause:
Replacement ATV212 installed into an S-Flex.

Resolution:
See the S-Flex manual to program the VFD in the section labeled Programming the Power Converter.
An excerpt of the current (10/2018) manual is attached.
After these initial settings are made, then program per application.

The complete manual is available for download here: https://www.se.com/us/en/download/document/30072-451-83/

Schneider Electric Saudi Arabia

Attachment(s)
S-Flex VFD factory settings.pdf [106.23 KB]