Search FAQs
Can Magelis HMI communicate with an Allen-Bradley CompactLogix 5370 PLC via 1769-L30ER?
Issue
I would like to read and write from my Magelis HMI to an Allen-Bradley CompactLogix 5370 PLC via 1769-L30ER module.Product Line
Vijeo Designer, Magelis HMI (XBTGT, XBTGK, XBTGH, HMISTU, HMISCU, HMIGTO, HMIGTU)Resolution
For the Magelis HMI to communicate to an Allen-Bradley CompactLogix 5370 PLC via 1769-L30ER module, use the Allen-Bradley Ethernet/IPIn the Vijeo Designer configuration software, the protocol can be added under the IO Manager node in the Navigator pane.
From the CompactLogix software, one can export an .L5K file and Link Variables to Vijeo Designer in order to sync the tags.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: