{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Troubleshooting AccuSine PCS+ Event Log Messages
Issue
User wishes to know what messages in the event log mean and how they should be addressed

Product Line
AccuSine PCS+

Environment
Event Log

Resolution
Please see the table below for a list of events one may see in the event log and the required action(s) to address.
EventExplanationAction
AC Line Not QualifiedFrequency Not QualifiedVerify Line Frequency is within ±3Hz.
Three Phase LossVerify AC Line is present.
Single Phase LossVerify all three line voltages are present.
Over VoltageVerify Line voltage is within +10%.
Voltage ImbalanceVerify voltage imbalance is less than 8%.
Fast Under VoltageVerify voltage is within 50% of nominal (1/4 cycle)
Fast Over VoltageVerify voltage is within +10% of nominal (1/4 cycle)
Auto Detection Out of RangeUnit was unable to Auto Detect voltage
or frequency
Disable Auto Detect. Manually enter nominal voltage and
frequency of the electrical system.
Low Order Harmonics OFF
[AHF type only]
5th and/or 7th order harmonic disabledTypically caused by harmonic loads without the minimum 3%
impedance or un-isolated power factor correction capacitors on
the load side of the main CTs
Fan Failure Detected Power section fan inoperable Call your local service center.
Filter Trip Inverter Filter inoperable Call your local service center.
Gate Drive Trip Power supply issue on Gate Driver Call your local service center.
HMI Communication Loss HMI communication to Control Board loss Verify Proper connection of HMI RJ45 Com jack.
Call your local service center.
IGBT Trip IGBT issue detected Call your local service center.
MOV Requires Service MOV issue detected Call your local service center.
Over Current Condition Detected Call your local service center.
Over Temperature Over Temperature detectedVerify air temperatures to the air intake of the unit are within
specification. Verify intake and exhaust air vents are not obstructed.
Parallel Power Wiring Mismatch L1, L2 and L3 are not powered by the same
phase for each parallel unit.
Ensure L1, L2 and L3 of all parallel units are powered by the same phase.
Protection Firmware Trip Firmware issue detected Call your local service center
Power Supply Out of Range Power Supply issue detected Call your local service center.
Current Sensor Inoperable Internal Current Sensor issue detected Call your local service center.
Transformer Over Temperature Transformer Over Temperature detected
(600 and 690 volt units only)
Verify air temperatures to the air intake of the unit are within specification.
Verify intake and exhaust air vents are not obstructed.
High Frequency Voltage Distortion Condition Excessive inverter switching frequency
detected on line voltage
Call your local service center.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.