Product Line
PM5000, PM8000, ION7650, ION8650 and ION9000
Environment
Meter Specifications
Resolution
Schneider Electric does not calibrate to C12.20, we verify to it. The ANSI C12.20 claim is as follows:
ION9000/ION8650 Accuracy Class 0.1 (0.1% energy accuracy at unity PF)
PM5000/PM8000/ION7650 Accuracy Class 0.2 (0.2% energy accuracy at unity PF)
PM5000, PM8000, ION7650, ION8650 and ION9000
Environment
Meter Specifications
Resolution
Schneider Electric does not calibrate to C12.20, we verify to it. The ANSI C12.20 claim is as follows:
ION9000/ION8650 Accuracy Class 0.1 (0.1% energy accuracy at unity PF)
PM5000/PM8000/ION7650 Accuracy Class 0.2 (0.2% energy accuracy at unity PF)
Released for:Schneider Electric Saudi Arabia