Below are the required minimum firmware versions in order to be compatible with a redundant M580 PAC.
Note: Though matching revisions is recommended, as long as the above minimum requirements are met, mixing versions is allowed.
Reference | Description | Minimum Firmware Version |
BMXCRA31200 | X80 Standard Drop Adapter | 2.14 |
BMXCRA31210 | X80 Performance Drop Adapter | 2.14 |
BMECRA31210 | X80 Performance Drop e-Adapter | 2.14 |
140CRA31200** | Quantum Ethernet Drop Adapter | 2.14 |
BMENOC0301 | M580 Ethernet Scanner | 2.04 |
BMENOC0311 | M580 FactoryCast Ethernet Scanner | 2.04 |
Note: Though matching revisions is recommended, as long as the above minimum requirements are met, mixing versions is allowed.
** Quantum drops are not supported with the BMEH582040.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)