{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the definition of ANSI 74 - Trip/closing circuit supervision?
To detect trip circuit and closing circuit failures, Sepam monitors:
  • shunt trip coil connection
  • closing coil connection
  • matching of breaking device open/closed position contacts
  • execution of breaking device open and close orders.
The trip and closing circuits are only supervised when connected as shown in attached photo.

Schneider Electric Saudi Arabia

Attachment(s)
ANSI 74.PNG.png [100.61 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.