{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME 9.0 new and updated device support

Product Line
PME 9.0
ION meter
Powerlogic meter


Environment

New and updated device support


Resolution

Following device support has been added to PME 9.0:
ItemDetails
PM8000 Modbus/ION coexistencePME 9.0 supports ION over Modbus
communications with PM8000 (v1.4.1+) devices.
ION9000 supportPME now supports the new high end ION9000
power monitoring device.
New device type supportThe following device types are now supported in
PME 9.0 :
  1. ION9000
  2. PM8000v2 (with ION over Modbus support)
  3. MTZ Wave 2 (support for breaker aging)
  4. EM4900
  5. PowerTag
  6. AccuSine PCSN
  7. IFL
  8. Galaxy VM/VX
  9. SmartLink IPZ
  10. Compact NSXm
  11. Com'X WAGES
Updated device license requirementsPM8000 and MTZ now require a DL-S license
(was DL-M before)

For the list of default supported devices, please refer to FA363561
For more information, please refer to PME 9.0 documentation FA358303

Schneider Electric Saudi Arabia