{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the total length requirements for the Hilti anchors used in IBC and OSHPD seismic anchoring?
Issue:
A customer wants to know the total anchor height.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
The IBC and OSHPD seismic documents only show hole depth. Customers need to know the how much anchor is needed above the floor too.

Resolution:

Attached is a link to the technical information for the Hilti Kwik bolts that are specified to be used. Based on the length of the anchor used and the depth of the hole drilled, you can determine the height from the floor to the top of the fastener from the chart provided on the Hilti Kwik spec sheet.

Schneider Electric Saudi Arabia

Attachment(s)
Technical-information-ASSET-DOC-LOC-1543424.pdf [1.81 MB]