Search FAQs
Where do I purchase the Lexium Integrated Drive with Reference Part Number ILS2K573S2212?
Issue
Where do I purchase the Lexium Integrated Drive with Reference Part Number ILS2K573S2212?
Product Line
Lexium ILS Integrated Drives
Resolution
The Lexium Integrated Drive with reference number ILS2K573S2212 is a special proprietary model specifically made for an OEM machine builder.
This model is proprietary to the OEM and is not available for purchase directly from Schneider Electric.
Please contact the OEM machine builder of the machine in which this motor is incorporated on to obtain a spare or a replacement.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: