{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does M580 NOP system comply to IEC62351-5
Question:
Does M580 NOP system comply to IEC 62351-5?

Answer:
IEC62351-5 is for secure authentication at power devices other than controllers. In terms of M580 NOP(IEC61850), it doesn't have encryption so not comply to this standard.
On the other hand, IEC62351 is for system and it can be addressed by power system…

Schneider Electric Saudi Arabia