Search FAQs
How to connect Analog Camera PAL/NTSC to Magelis GTU with Open box HMIG5U2?
Goals and Symptoms
Our Magelis HMIGTU ranges do not have the video input interface but the plan is to substitute the old XBTGT Multi Media series by these new HMIGTU series.
The goal of this resolution is to provide a way to connect Analog camera to Magelis HMIGTU.
Causes and Fixes
To substitute old XBTGT MultiMedia, we have done successful tests with Analog camera on Magelis GTU.
Using a Analog/ USB converter from Imaging Source Company (ref = DFG/USB2pro) you can connect Analog Camera PAL/NTSC to Magelis GTU with Open box HMIG5U2.
This converter is distributed worldwide.
VJD 6.2 SP8 HF01
Note: This Hotfix is only VJD Runtime installer and the runtime version is the same as SP8
Our Magelis HMIGTU ranges do not have the video input interface but the plan is to substitute the old XBTGT Multi Media series by these new HMIGTU series.
The goal of this resolution is to provide a way to connect Analog camera to Magelis HMIGTU.
Causes and Fixes
To substitute old XBTGT MultiMedia, we have done successful tests with Analog camera on Magelis GTU.
Using a Analog/ USB converter from Imaging Source Company (ref = DFG/USB2pro) you can connect Analog Camera PAL/NTSC to Magelis GTU with Open box HMIG5U2.
This converter is distributed worldwide.
- You can re-use the Vijeo Designer XBTGTxx40 application and to convert it on HMIG5U2 Box with selection of the same display size than XBTGT !
- You have same Video functions: Live Video Display, Record & Replay functions
- You have also to install manually on the HMIG5U2 the Windows drivers by installing Vijeo Designer Runtime of V6.2 SP8 HF01.
VJD 6.2 SP8 HF01
Note: This Hotfix is only VJD Runtime installer and the runtime version is the same as SP8
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: